Configuring a WITS State Counter Point

In ClearSCADA, a WITS State Counter Point database item represents a State Counter point in a WITS Field Device. You use it to count the number of specific state changes that have occurred for a particular point (the parent point) in a particular period.

An example use might be to count the number of times a pump has been started each day. The Field Device stores the count in the State Counter point. The count is the total count since the start of the current period. At the start of the next period, the Field Device resets the count to zero.

The State Counter Point is a virtual counter point. It is also a derived point. That is, it derives its value by performing a calculation on the value of another point (the parent point) (see Derived Points in the ClearSCADA Guide to Core Point Configuration).

WITS State Counter Point database items have a combination of configuration properties that are:

 

To configure a WITS State Counter Point database item, you use the WITS State Counter Point Form.

The configuration Form contains many fields, organized into tabs. Some of these tabs contain properties that are common to points on many drivers (see Tabs on Point Forms in the ClearSCADA Guide to Advanced Drivers).

 

The State Counter tab contains properties that are specific to WITS. Use the fields on the tab to:

 

When you have completed the point's configuration, you need to download the configuration to the Field Device by using the Outstation database item's Download Configuration (WITS Outstation) action.

If your Field Device does not support configuration download, you will need to make the same changes to the Field Device's configuration locally.


Disclaimer

ClearSCADA 2017 R3