Configure a Multi-Monitor Setup

To launch the ViewX Client on a Multi-Monitor setup, you need to create a Startup Configuration File.

The configuration file needs to be named 'StartupConfiguration.xml'and placed in the following directory:

C:\ProgramData\Schneider Electric\ClearSCADA

If this file is detected when the ViewX client launches, its settings are applied to the Multi-Monitor setup.

If the XML in the Startup Configuration File is not valid, a diagnostic message will appear when you launch the ViewX Client (see Resolve an Invalid Startup Configuration File).


Disclaimer

ClearSCADA 2017 R3