WebX and XML Client - System Connections

ClearSCADA supports remote access via WebX clients and Third Party XML clients. WebX clients are client PCs that run the WebX application supplied by Schneider Electric and Third Party XML clients are client PCs that are running an XML application not supplied by
Schneider Electric. Both types of client provide remote access to your system by connecting, via Internet or Intranet, to a web server that is installed on the ClearSCADA server.

WebX clients and Third Party XML clients can be used at any location where Internet/Intranet access is provided and are easy to set up.

However, there are some limitations with WebX and XML clients:

In the following sections, we describe how WebX/XML client - system connections work and explain how to connect to ClearSCADA via WebX/XML.


Disclaimer

ClearSCADA 2017 R3