Print a Previously Generated Report

You can print a report that is displayed in the Crystal Reports Viewer by using the Print Setup and Print options from the ViewX File menu. You can also print reports from within the Crystal Reports Viewer.

Be aware that any print settings specified on the report’s configuration Form do not apply when printing a report directly from the Crystal Reports Viewer—instead, you need to specify the required settings using the Print Setup option on the ViewX File menu.

If you use the Crystal Reports Viewer to print a report, be aware that the report content will not contain the latest ClearSCADA data. Instead, the report that you print will contain data that has been previously retrieved using the Generate Report pick action.


Disclaimer

ClearSCADA 2017 R3