ClearSCADA Parameters

You can add Parameter database items to ClearSCADA. You can use such Parameters for storing static data values, such as map grid references. Parameters are internal to ClearSCADA and are designed to store data that is not directly associated with other items in the database (such as individual points, outstations, or scanners). You can use Parameters as an alternative to Custom Configuration Fields, if the values that need storing are not directly associated with other items in the ClearSCADA database.

To include ClearSCADA Parameter data in your reports, you need to either include the Parameters in a Data Grid, or as a subreport (see Use a Subreport to Include Unrelated Data in the Same Report).

For more information on configuring ClearSCADA Parameters, see Using Parameters to Store Static Data Values in the ClearSCADA Guide to Core Configuration.

Do not confuse ClearSCADA Parameters with Crystal Reports’ Parameters (see Parameter Field).


Disclaimer

ClearSCADA 2017 R3