Define the Text Font Settings for a Mimic

You can use the Text Font tab of the Mimic Properties window to define the default settings for the style, size and orientation of the lettering in text boxes that you add to Mimics. This is useful when you know that you need to add multiple text boxes to a Mimic, each with the same style of lettering. Rather than configure the font settings for each text box separately, you can define the default font settings for text boxes. After doing this, each text box that you add will already have the default font settings in place. You can make further adjustments to each text box by configuring its own settings separately if required.

Depending on the method that you use to display the Mimic Properties window, the settings you define will be applied to:

When you have displayed the Mimic Properties window using the appropriate method for your needs, define the Text Font settings as required. The various Text Font settings work in the same way as the similarly named settings on the Font tab of the Text Properties window (see Editing a Text Box).


Disclaimer

ClearSCADA 2017 R3