Editing a Mimic Parameter

You can change the configuration of any Mimic parameter as required. To edit a parameter:

  1. Display the Parameters window (see Displaying the Parameters Window).
  2. Select the parameter that you want to edit.
  3. Select the Edit button to display the Edit Parameter window.
  4. Alter the settings on the Edit Parameter window as required, then select the OK button to confirm. The settings on the Edit Parameter window work in the same way as the corresponding settings on the Add Parameter window.

Disclaimer

ClearSCADA 2017 R3