Configuring Analog Points

The Performance Monitor driver uses Performance Monitor Analog Input points to reference the individual system performance attributes that it is to monitor, and to define how that performance data is to be managed within ClearSCADA.

This section covers configuration of properties on the Performance Monitor tab of the Form (see Configure the Performance Monitor Properties). Configure the properties of each analog point using the fields on the Performance Monitor Analog Point Form.

You need to configure a separate Performance Monitor Analog point for each performance attribute that you want to monitor on a particular node.

Example:

Two Performance Monitor Analog points monitor aspects of performance on a ClearSCADA server.

One analog point monitors the available bytes of memory on the server, and raises an alarm if this drops below a certain percentage.

Another analog point monitors the available disk space on the server, and is configured to raise an alarm when the disk containing the historic data reaches 75% full. The alarm indicates that the amount of historic data being stored is too great and may need to be reduced (for example, by reducing the data’s life time, or re-configuring some points to store less historic data).

Further Information

For information on the fields on the Analog Point tab, see Defining Analog Point Details in the ClearSCADA Guide to Core Point Configuration.

For information on the fields on other tabs, see Tabs on Point Forms in the ClearSCADA Guide to Simple Drivers.

For more information on configuring Performance Monitor points to monitor the free disk space on each of the servers on a ClearSCADA system, see Monitor the Available Disk Space in the ClearSCADA Guide to Server Administration.


Disclaimer

ClearSCADA 2017 R3