Archive Status Display

You can use the Archive Status Display (also referred to as the Archive View Window) to access information about the current status of an archive. This is useful for checking the progress of the archive operations.

Access the Status Display as you would other Status Displays, (see View a Status Display in the ClearSCADA Guide to ViewX and WebX Clients).

The Status Display varies in appearance according to the type of interface that you use to access the display as well as the following:

The Status display for an Archive includes the following archive-specific status attributes:


Disclaimer

ClearSCADA 2017 R3