Standby Tab

Use the Standby tab to configure the settings for the connection between the server on which you are working and the other Main and Hot Standby servers in the architecture.

The Standby tab’s settings are arranged in columns, with settings for Standby A and settings for Standby B (only available when the Type is set to Hot-Standby Pair or Triple Standby). Use the Standby A column settings to configure the connection between the server and one of the other Main/Hot Standby servers in the architecture. (A Hot Standby server is a server that may become either the Main server or remain a Standby server). On Triple Standby systems, the Standby B settings can be used to define the connection to the other Main/Hot Standby servers in the architecture.

The Standby tab contains the following sections:


Disclaimer

ClearSCADA 2017 R3