Data File Cache

The Data File Cache category shows statistical information about the data files that are used by Data Tables, Crystal Reports definition files, the latest Crystal Reports data files, and some other driver-specific files. The data that is used in the Data Tables, Crystal Reports definition files, and so on, is stored in Data Files. When the data in the files is required, the relevant data files are loaded into memory. If changes are made to the data files while they are loaded in memory, ClearSCADA will attempt to flush these changes so that they are stored in the data files on disk.

The Data File Cache statistics are displayed under these categories:

Further Information

Location of the Data Files: see Locations of the Database Folders in the ClearSCADA Guide to Server Administration.

Define the Cache and Flushing settings for Data Files: see Data Files Settings in the ClearSCADA Guide to Server Administration.


Disclaimer

ClearSCADA 2017 R3