Client PC Requirements

When purchasing clients for use with ClearSCADA, there are many factors you need to consider, including the operating systems supported by ClearSCADA and the type of displays required.

In the following sections, we describe the recommended specifications for clients that are to use ClearSCADA:

You should also refer to the following sections, which apply to both ClearSCADA servers and ClearSCADA clients:


Disclaimer

ClearSCADA 2017 R3