Database Objects

After the driver is installed, you can create ROC database objects (‘database items’) in the usual way. To add a ROC-specific database object, right-click on a Group in the Database Bar, select Create New, then ROC Plus, and then the type of object that you want to create.

 

Each object includes settings and properties that are common to many Geo SCADA Expert objects, like Alarm Redirection, User Methods, Identification, point Alarm Limits, and so on. For information on these common properties, see Configure a New or Existing Point in the Geo SCADA Expert Guide to Core Point Configuration. For information about settings and properties that are ROC-specific, see the topics listed below:

 

For Geo SCADA Expert to interface with a supported ROC device, as a minimum you need to configure: 1 ROC Plus Channel, 1 ROC Plus Scanner, and 1 ROC Plus Point in your database.

In addition to using ViewX and Virtual ViewX, you can also view information about each database object in the Geo SCADA Expert Database Schema. The view in the schema shows the properties and methods for the object.

Further Information

Data Tables are generic database objects.

For information about configuring a Data Table to hold ROC events, (see Event Data Table).

For information about configuring a Data Table to hold ROC alarms, (see Alarm Data Table).


Disclaimer

Geo SCADA Expert 2020