Delete Reference Dynacard Data
Associated with: Dynacard Stores
Security permission required to access this pick action: Diagnostics
LOSS OF REFERENCE DATA
Use the Delete Reference Dynacard Data pick action with care. Once triggered, the pick action will permanently delete the ‘Reference’ data that is stored in Geo SCADA Expert for the selected Dynacard Store.
Use this pick action to permanently delete the data that is currently stored as the ‘Reference’ data against which other dynamometer data is compared. Use the pick action, for example, if the existing set of ‘Reference’ data is misleading or inaccurate.
(To merely replace the existing set of ‘Reference’ data with more suitable data, you only need use the Copy a Stored Card to Reference Card pick action.)