Configuring Digital Points

Use Advanced EWS Digital Points to map digital ‘point’ data on Advanced EWS servers into Geo SCADA Expert in a suitable format, and vice versa.

Configure the properties of each Digital point using the fields on the Advanced EWS Digital Point Form.

This section covers configuration of the digital-specific properties on the Digital Point tab of the Form.

Use the Digital Point tab to:

For information about the Digital Point tab on the Digital Point Form, see Defining Digital Point Details in the Geo SCADA Expert Guide to Core Point Configuration.

If the point is a digital output point:

Properties on other tabs are common to many points, see Tabs on Point Forms in the Geo SCADA ExpertGuide to Advanced Drivers.


Disclaimer

Geo SCADA Expert 2020