Add a Calendar

To add a Calendar:

  1. Right-click on the System or Group to which you want to add the Calendar (this might be a separate Group for storing Calendars).
    A context-sensitive menu is displayed.
  2. Select the Create New option.
    A further menu is displayed.
  3. Select the Other option.
    A further menu is displayed.
  4. Select the Calendar option.
    A Calendar is added to the system. It is selected automatically, ready for you to enter its name.
  5. Enter a suitable name for the item (taking into account the Geo SCADA Expert Naming Restrictions).
  6. Select another part of the interface or press the Enter key to confirm the entry.

When you have added a Calendar, you can:

Do not confuse ‘normal’ Calendars with Alarm Redirection Calendars that can be used to redirect alarms on a calendar basis. For information on Alarm Redirection Calendars, see the Geo SCADA Expert Guide to Alarm Redirection.


Disclaimer

Geo SCADA Expert 2020