Configure the Slave’s Security Properties
            Use the fields on the Security tab of each DNP3 Slave Outstation Form to specify properties that relate to DNP3 Secure Authentication when Geo SCADA Expert is operating as a DNP3 Slave.
Use the fields on the Security tab to:
- Specify Whether DNP3 Secure Authentication is Used
 - Specify the Algorithms used to Secure Message Content
 - Specify When the Slave Outstation is to Invalidate its Pair of Session Keys
 - Specify Whether Aggressive Mode is Used
 - Specify the Maximum Error Count
 - Define Whether the Slave Outstation Logs Authentication and Key Change Information.