Configure Digital Points

Use an EtherNet/IP Digital Point to map an item of data (a tag) in the controller to a digital point in Geo SCADA Expert database. You do this when the tag comprises digital data to enable Geo SCADA Expert to represent that data in the database.

You configure the properties of each digital point using fields on the EtherNet/IP Digital Point Form. The configuration Form contains many fields, organized into tabs. Most of these tabs contain properties that are common to points on many drivers (see Tabs on Point Forms in the Geo SCADA Expert Guide to Advanced Drivers).

This section covers configuration of the digital point-specific properties on the Digital Point tab of the Form.

Use the Digital Point tab to:

With each digital point that is to operate as an output point (in order to control plant), you also have to enable and configure the properties on the Control tab. For more information, see Define the Control Settings for a Digital Output Point in the Geo SCADA Expert Guide to Core Point Configuration.

Further Information

Minimum Configuration - Points.


Disclaimer

Geo SCADA Expert 2020