Station Counter Interrogation Alarm
Associated with: IEC 60870-5 outstations
This attribute indicates whether the latest Request, Freeze and/or Reset request for the outstation’s counters has been unsucessful (see Understand and Resolve Outstation Interrogation Alarms).
The frequency with which Geo SCADA Expert attempts to execute the above requests is specified as part of the outstation’s configuration (see Configure the Counter Interrogation Intervals).
Possible states: Displays one of the Standard Alarm States.