System Analysis
This section is designed for use by system administrators and high-level engineers when assessing the state of the Geo SCADA Expert system. It describes the statistical and diagnostic information provided specifically for the IEC 60870-5 driver. For more general information on analyzing a Geo SCADA Expert system, see System Analysis in the Geo SCADA Expert Guide to the Server Status Tool.
During system analysis, you might need to:
- Adjust the Configuration of any IEC 60870-5 Points that Cause a High Load
- Driver Logging Options that are Specific to the IEC 60870-5 Driver.
Additionally, if an outstation is not communicating with the server when it should be, see Troubleshooting in the Geo SCADA Expert Guide to Advanced Drivers.
When troubleshooting on a Geo SCADA Expert system, examine the diagnostic messages in the Events List. The messages may help you to identify the cause of any problems.
Further Information