Common Point Properties
Use the fields at the top of the Analog Point tab to Configure Common Point Properties. Fields that are specific to analog points are explained below.
Only applies to Hardware I/O types. Use the Channel Number field to specify the channel number for the point, in the range 1 to 8.