Last Outstation Event
Associated with: Lufkin SAMS controllers
This status attribute displays information about the latest controller event to be uploaded to Geo SCADA Expert. The information includes:
- The Lufkin-defined Id that identifies the type of outstation event
- A description of the event (if available)
- The date and time at which the controller logged the event.
The status attribute is displayed once Geo SCADA Expert has retrieved an event from the controller’s Event Log (see Upload Event Log).The status attribute provides information about the controller event that has the latest time stamp in the collection of controller events that Geo SCADA Expert last uploaded. (For information about earlier controller events, see the Events List.)
Example:
Id: 27, Description: "Gauge Off Time Changed", occurred at 25/Jul/2012 11:42:45.000