Introduction to the MQTT JSON Schema A Driver
This driver is an extension driver. It provides additional application-specific functionality to the 'parent' driver with which it is associated. To interact successfully with devices using an extension driver, you need to:
- Install and run both the extension driver and its 'parent' driver (and, if applicable, its 'grandparent' driver)
- Ensure that  the extension driver and its 'parent' driver (and, if applicable, its 'grandparent' driver) are licensed
 (some extension drivers are licensed separately to their 'parent' driver)
- Configure the required database items and settings on the 'parent 'driver (and, if applicable, the 'grandparent' driver)
- Configure the required database items and settings on this extension driver.
- Ensure that the database items (and any database items on which they depend) have valid, saved, configuration and are 'In Service'.
Intended Audience
This guide is primarily intended for engineers who are responsible for configuring MQTT JSON Schema A driver items and features in the Geo SCADA Expert database.
The guide also contains information for maintenance engineers.
Document Scope
This guide explains the configuration, features and database items that are specific to Geo SCADA Expert’s MQTT JSON Schema A driver. The driver enables Geo SCADA Expert to retrieve data using either of two MQTT JSON Schema A message formats.
 Prerequisite Reading
Prerequisite Reading
                This guide contains technical information that is intended for users that are sufficiently familiar with Geo SCADA Expert configuration and operation. Before reading this driver guide, ensure that you are familiar with:
- Geo SCADA Expert configuration practices, procedures, and the configuration of properties that are common to many database items. For more information, see the Geo SCADA Expert Guide to Core Configuration, and the Geo SCADA Expert Guide to Core Point Configuration.
- Driver structure, components, and configuration properties, pick actions, and status attributes that are common to many drivers. For more information, see the Geo SCADA Expert Guide to Drivers.
- The database items and configuration that are specific to this extension driver's 'parent' driver, along with any pick actions, status attributes, and logging options that are specific to that 'parent' driver. (Unless stated otherwise, this extension driver supports the features and options that are supported by its 'parent' driver, in addition to the features and options that are described in this extension driver guide.)
Some sections of this guide are intended for operator-level users. These sections are intended for users that are familiar with the navigational and operational aspects of Geo SCADA Expert. Before reading the operational sections in this guide, ensure that you are familiar with:
- The Geo SCADA Expert user interfaces (ViewX and Virtual ViewX), the various types of display, their navigation and operation. For more information, see the Geo SCADA Expert Guide to ViewX and Virtual ViewX Clients.
POTENTIAL SECURITY BREACH
The MQTT JSON Schema A driver is an MQTT extension driver. It provides additional functionality to enable Geo SCADA Expert to retrieve data using either of two MQTT JSON Schema A message formats (see Supported Message Formats).
In order to retrieve data using the MQTT JSON Schema A message formats, Geo SCADA Expert needs to run both the MQTT driver and the MQTT JSON Schema A extension driver (see Confirm that the MQTT JSON Schema A Server Component is Installed).
Use this Geo SCADA Expert Guide to the MQTT JSON Schema A Driver alongside the Geo SCADA Expert Guide to the MQTT Driver. As much of the information in the latter guide is assumed knowledge, we recommend that you read the Geo SCADA Expert Guide to the MQTT Driver before reading this driver guide.