Configuring a Map Source

A Map Source represents the origin of a layer on a Geo SCADA Expert map. The Map Source can be online (on the internet) or offline (not on the internet). For example, a layer could be the OpenStreetMap® world map or an overlay graphic showing wind speed and direction data from an open source server. To create a map, you specify and then combine one or more Map Sources (layers) to create a Map Set, which users can then display as a multi-layered composite map. For more information, see Creating a Geo SCADA Expert Map and see Creating a Map Set.

Each Map Source is represented in the Geo SCADA Expert database by a Map Source database item.

Geo SCADA Expert currently provides access to a number of different Map Sources (see Which Map Sources does Geo SCADA Expert Support?).

To create a Map Source database item, see Creating a Map Source.

Once you have created a new Map Source item, you then need to define its settings. To do this, right-click on the item to display its Object Menu then select the Edit Properties option.

Geo SCADA Expert will then display the Map Source form:

This section describes the settings on the Map Source tab of the Map Source form.

You can find details of the settings on the other tabs as follows:

Use the Map Source tab to set the various properties of a Map Source. Each source has different settings such as:

For more information, there is a topic for each of the standard Geo SCADA Expert Map Sources. Select the appropriate topic in the gray footer section at the bottom of this topic.


Disclaimer

Geo SCADA Expert 2020