Creating a Geo SCADA Expert Map

You can create single-layer maps or multi-layer composite maps in Geo SCADA Expert, from online or offline mapping sources, which you can then use for a variety of purposes. For example, you can display:

To create a map:

  1. The first step is to specify the source of each map layer (for more about map layers, see About Geo SCADA Expert Maps). You do this by creating and configuring a Map Source database item for each layer. Geo SCADA Expert currently provides access to a number of different Map Sources (see Which Map Sources does Geo SCADA Expert Support?). OpenStreetMap® and Bing Maps® provide base layer maps while ArcGIS® and WMS maps provide a wide range of both base layer and overlay mapping.

    For more information about creating and configuring a Map Source, see Creating a Map Source and see Configuring a Map Source.

  2. If you are creating a multi-layer map, with a base layer and overlays, the next step is to create and configure a Map Set database item. The Map Set item will contain a list of all the Map Sources (layers) in your composite map and represents the finished map. If you want, you can provide your users with a choice of base layers and overlays (for more about layers, see Using a Geo SCADA Expert Map).

    For more information about creating and configuring a Map Set, see Creating a Map Set and see Configuring a Map Set.

    For an example of how you can create a multi-layered map, with a choice of base layers and overlays, see Example - Creating a Multi-Layered Composite Map.

Once you have created your map, your users can then display it in Geo SCADA Expert (see Displaying a Geo SCADA Expert Map) and use the map (see Using a Geo SCADA Expert Map).


Disclaimer

Geo SCADA Expert 2020