Specify an Outstation Telephone Number
Use the Telephone Number property on the SCADAPack 50 tab to specify the telephone number of the device modem. Geo SCADA Expert can potentially receive messages from many devices. The Telephone Number and Outstation Name together identify to Geo SCADA Expert which device this is (see Specify an Outstation Name).
- Telephone Number—Specify the telephone number associated with the SIM card in the device modem. Use the required format. The format of the telephone number depends on the service provider (see the SIM card documentation for more information). An example format might be: +447867512345.