Resume Polling
Associated with: SCADAPack controllers on which Suspend Polling is enabled
Security permission required to access this pick action: Diagnostics
The Remote Connection interface is typically used to suspend or resume polling of a SCADAPack controller. However, if Suspend Polling is enabled, you can use the Resume Polling pick action to abort any current polling suspension and resume normal polling of a controller.
The Resume Polling pick action is only available for controllers on which the ‘Suspend Polling’ feature is enabled (see Specify Whether Geo SCADA Expert can Suspend Polling of a Controller).
Use the Resume Polling pick action to force polling to resume, regardless of whether polling was suspended via the Suspend Polling pick action, or the Remote Connection interface.