SCADAPack Point Addressing
SCADAPack controllers support one of two point address ranges—5 Digit, or 6 Digit. You need to be aware of which address range each controller on your system supports. (For instance, current SCADAPack controllers use 5-Digit addressing.) Specify the supported Point Address Range on each SCADAPack Outstation Form .
Specify the individual point Address on each SCADAPack Modbus Point Form (see Configure Common Point Properties). Points on SCADAPack controllers use addresses within the 5- and 6-Digit address ranges listed below. Be aware that each type of controller has its own specific address range—refer to the controller documentation for the address range that applies to a specific type of controller.
| Modbus Data Type | Geo SCADA Expert Point Type | 5-Digit Address Range | 6-Digit Address Range |
|---|---|---|---|
|
Coil, |
Digital Output Point, Digital Input Point |
1 to 9999 |
000001 to 099999 |
|
Discrete Input |
Digital Input Point |
10001 to 19999 |
100001 to 199999 |
|
Input Register |
Analog Input Point, Digital Input Point |
30001 to 39999 |
300001 to 365536 |
|
Holding Register |
Analog Output Point, Digital Output Point, Analog Input Point, Digital Input Point |
40001 to 49999 |
400001 to 465536 |
Further Information
Modbus Function Codes Supported by the Geo SCADA Expert SCADAPack Modbus Driver.