Actions Associated with SCADAPack Modbus Flow Runs
            These actions are specific to SCADAPack Modbus Flow Runs:
- Abort Orifice Plate Change—Dual Chamber Orifice Plate Changes
 - Alarm Log Demand Poll
 - Batch Records Demand Poll
 - Change Gas Composition Ratios—AGA-8 only
 - Daily Demand Poll
 - Event Log Demand Poll
 - Force Inputs
 - Hourly Demand Poll
 - Normalize—AGA-8 only
 - Orifice Plate Change—AGA-3 only
 - Read Configuration
 - Reset Sensor Statistics
 - Start Orifice Plate Change—Dual Chamber Orifice Plate Changes
 - Write Configuration.