Configure the Flow Run Properties
            For each type of Flow Run use the fields on the Flow Run tab of the Flow Run Form to:
You can configure these properties directly in Geo SCADA Expert, or read the configuration into the Geo SCADA Expert database (see Configure or Read the Flow Run Configuration).
With the properties listed below, you can either Configure or Read the Flow Run Configuration.