Realflo Specific Status Display Attributes
            This driver is an extension driver. As such, it supports a combination of the status attributes that are supported by its 'parent' driver, in addition to its own driver-specific status attributes. Use this section in conjunction with the 'parent' driver documentation for comprehensive information about the status attributes that are supported by this extension driver.
                
Further Information
Status attributes supported by this driver's parent driver: see SCADAPack Modbus Specific Status Display Attributes in the Geo SCADA ExpertGuide to the SCADAPack Modbus Driver.