Other Channel Configuration Fields
Some Totalflow Channel configuration fields do not appear on the configuration form but are listed in the Geo SCADA Expert Database Schema.
- Logging Level—This tag controls the level of detail in the driver module’s log file for actions related to this channel. A value of 0 means that the log file contains errors only and a value of 4 means that the log file is extremely verbose. For more information on logging, see Driver Log File.