Remove a File from a SCADAPack E Outstation’s Configuration

Use the Remove button on the Configuration Setup Window to remove a file from the SCADAPack E outstation.

To remove a file:

  1. Select the file’s entry in the Configuration Setup window.
  2. Select the Remove button.
    A confirmation dialog box is displayed.

  3. Select Yes to remove the file from the list in the Configuration Setup Window.

    (Select No to keep the selected file.)

  4. Select the OK button on the Configuration Setup window.
    If ‘Yes’ was chosen in step 3, the specified file is removed from the DNP3 SCADAPack E outstation in Geo SCADA Expert database.

Removing a file from the DNP3 SCADAPack E outstation in the Geo SCADA Expert database does not remove the file from the SCADAPack E outstation’s file system.

To remove a file from the outstation’s file system:


Disclaimer

Geo SCADA Expert 2020