Restrict Alarm Access

Access to alarms or alarm-related actions can be restricted:

In addition to the above, a Default Alarm Filter can be used to present a subset of alarms to a user (see Specify a Default Alarm Filter). If required, the user can change this initial filter to display further alarms to which they have access.


Disclaimer

ClearSCADA 2017 R2