Secondary Window Container

Secondary Window Containers display document windows in Run Mode or Design Mode, allowing database items such as Mimics, Lists, Trends or reports to appear simultaneously on separate monitors. A Multi-Monitor setup supports up to 5 Secondary Window Containers.

You can configure a Secondary Window Container to:

If a container supports multiple documents, each document window appears with its own tab.

Secondary Window Containers can also display the Alarm Banner or they can be configured to display the Alarm Banner in Full mode (see Launch the Alarm Banner in Full Mode).


Disclaimer

ClearSCADA 2017 R2