Specify the Data Set Field Properties

When you add new fields to a Data Set, you need to specify the properties for each field.

The Edit Field window allows you to define the properties for a new field or edit the properties for an existing field in a Data Set.

The Edit Field window contains these fields:


Disclaimer

ClearSCADA 2017 R2