Configuring Control Checks Settings

You can do the following checks on the control feedback from a device:

You can perform these checks for the analog and digital output points associated with devices as well as pulse controls. For more information about sending controls to a device from output points, see Introduction to Points. ClearSCADA will only make the Uncommanded Change check if the output point has been successfully controlled at least once.

To monitor feedback input from the device, you can:

You then use the fields on the Control Checks tab of the relevant output point form to set up the feedback check.

The fields are divided into two sections. A section for the Control Feedback check and a section for Uncommanded Change check. To enable the fields, you need to select the Enabled check box at the top of the Form.

You can now use the Control Feedback Settings and the Uncommanded Change Settings fields.

For worked examples of how to configure a Control Feedback check or an Uncommanded Change check, see Worked Example - Configuring a Control Feedback Check or see Worked Example - Configuring an Uncommanded Change Check.


Disclaimer

ClearSCADA 2017 R2