Define Whether a Counter-Type Point can be Overridden

You can use the Point Form for a counter-type point to define whether the point’s value can be overridden. You can also define the range of valid override values.

The Override pick action allows users whose User Accounts are allocated the Override/Release permission for a point to define the value of that point. The override feature is useful when a known detected fault is resulting in an incorrect value being reported for a point—an operator can temporarily override the value back to a suitable value until the detected fault has been corrected. Overrides can also be used to simulate different plant states when testing the system.

However, you may require that a point value cannot be overridden. When the Override feature is disabled, ClearSCADA continues to use the point’s actual value—the value reported by the outstation, PLC, or other device on which the point is located—regardless of the state of that device.

To configure the override feature for a counter-type point:

  1. Display the Form for the counter point that you want to configure (see Display a Form in the ClearSCADA Guide to Core Configuration).
  2. Select the <Point Type> tab (for example, the Counter tab for a DNP3 Counter point).
  3. Use the Enabled check box in the Override section to define whether the point can be overridden:

    Either:

    • Select the Enabled check box in the Override section to enable the Override feature.
      The Maximum and Minimum fields become available. Use the fields to define the override range (proceed to step 4).

      or:

    • Clear the Enabled check box to disable the Override feature.
      The Maximum and Minimum fields are grayed out. The point cannot be overridden (ignore step 4).
  4. Use the Maximum and Minimum fields to define the override range. The range defines the values that operators can enter to override the point—any value between and including the minimum amount and the maximum amount.
    1. In the Maximum field, enter the highest value that operators can use to override the point.
    2. In the Minimum field, enter the lowest value that operators can use to override the point.
  5. Use the Confirm combo box to define whether a confirmation dialog box is displayed whenever an operator requests that a point is overridden (see Requesting Confirmation of Action Requests in the ClearSCADA Guide to Core Configuration).
  6. Save the configuration (see Saving Configuration Changes in the ClearSCADA Guide to Core Configuration).

If you enable the Override feature, ensure that the point’s Override/Release security permission is suitably set (see Allocating Security Permissions in the ClearSCADA Guide to Security).


Disclaimer

ClearSCADA 2017 R2