Waiting For Feedback

Associated with: Analog output points, digital output points and pulse controls for which a feedback point has been configured.

ClearSCADA will set the attribute to True if the feedback point is waiting for an input value, otherwise ClearSCADA will set the attribute to False.

For more information, see Configuring Control Checks Settings and see Control Feedback Settings.

Example:

False.


Disclaimer

ClearSCADA 2017 R2