Introduction to the FloBoss Driver

This driver is a simple driver. It provides additional functionality to enable ClearSCADA to interface with specific supported devices using a particular protocol. To interact successfully with such devices, you need to:

ClearSCADA is a flexible and extensible SCADA host platform that can be used for a multitude of purposes, including gathering data from and controlling remote devices. The ClearSCADA FloBoss Driver extends the core functionality of ClearSCADA to enable it to communicate with supported Emerson FloBoss Flow Computers, using the ROC Protocol.

Intended Audience

This guide is intended for engineers that are tasked with configuring ClearSCADA to communicate with supported Emerson FloBoss Flow Computers using the ROC Protocol.

The guide assumes an advanced level of expertise with ClearSCADA, Microsoft Windows, electronic flow measurement, and FloBoss Flow computers.

Document Scope

This guide explains how to install and configure database objects on the ClearSCADA FloBoss Driver and provides information about the example configuration that is available for importing into your database from a ClearSCADA database export (sde) file.

The ClearSCADA FloBoss driver provides a subset of the features that are available using Emerson’s custom ROC Protocol, with a bias towards gathering historical data from FloBoss flow computers.

With the ClearSCADA FloBoss driver, you can:

The level of technical information in this guide is for users who have an advanced level of expertise with ClearSCADA, Microsoft Windows, electronic flow measurement and FloBoss flow computers.


Disclaimer

ClearSCADA 2017 R2