Introduction to the Lufkin SAMS Driver

This driver is an extension driver. It provides additional application-specific functionality to the 'parent' driver with which it is associated. To interact successfully with devices using an extension driver, you need to:

Intended Audience

This guide is primarily intended for engineers who are responsible for configuring Lufkin SAMS items and features in the ClearSCADA database.

The guide also contains information for operators and engineers who use the Lufkin SAMS driver to monitor rod pump activity.

Document Scope

This guide explains the configuration, features and database items that are specific to ClearSCADA’s Lufkin SAMS driver. The driver is an Advanced Modbus extension driver. The driver provides additional functionality to enable ClearSCADA to interface with Lufkin SAM rod pump controllers. The driver enables ClearSCADA to communicate with the controllers using the Modbus protocol with proprietary extensions. Using the driver, ClearSCADA can retrieve and process rod pump stroke and other data associated with monitoring the effectiveness of the rod pumps that are being used to lift liquid out of wells. The uploaded dynacard data can then be displayed as a series of Dynagraphs that users can analyze to determine the effectiveness of the pumps in the well fields.

In order to communicate with Lufkin SAM controllers, ClearSCADA needs to run both the Advanced Modbus driver and the Lufkin SAMS extension driver (see Confirm that the Lufkin SAMS Server Component is Installed).

Use this ClearSCADA Guide to the Lufkin SAMS Driver alongside the ClearSCADA Guide to the Advanced Modbus Driver. As much of the information in the latter guide is assumed knowledge, we recommend that you read the ClearSCADA Guide to the Advanced Modbus Driver before reading this driver guide.

The Lufkin SAMS driver documentation explains how to:

It also explains features that are of interest to operators, such as:

System administrators and engineers who are investigating unexpected behavior relating to the Lufkin SAMS driver might wish to refer to the following section:

For further information on Lufkin SAM devices, or on analyzing rod pump data, please refer to the documentation provided with the Lufkin SAM controllers and well field equipment.


Disclaimer

ClearSCADA 2017 R2