Arrange Command Group

The Graphics Tab includes the Arrange command group, which you can use to control how Mimic objects are placed on the Mimic background. You can also use it to group and un-group Mimic objects.

Certain commands in the Arrange group are only available when a minimum of two or three Mimic objects are displayed or currently selected. The Arrange commands include:


Disclaimer

ClearSCADA 2017 R2