Introduction to the Mitsubishi Driver
This driver is a simple driver. It provides additional functionality to enable ClearSCADA to interface with specific supported devices using a particular protocol. To interact successfully with such devices, you need to:
- Install and run the driver
- Ensure that the driver is licensed
- Configure the required database items and settings on the driver
- Ensure that the database items (and any database items on which they depend) have valid, saved, configuration and are 'In Service'.
Intended Audience
This guide is primarily intended for engineers who are responsible for configuring Mitsubishi items and features in the ClearSCADA database.
The guide also contains information of use to maintenance engineers.
The Mitsubishi Driver provides extra functionality to allow a ClearSCADA system to be populated with data from, and control points on, Mitsubishi Slaves or Mitsubishi PLCs. The driver allows ClearSCADA to communicate with:
- Mitsubishi Slaves
- The MELSEC A range of MitsubishiTM PLCs
(using Transmission Control Protocol Format 1) - Third-party PLCs that communicate using the Mitsubishi MELSEC A protocol.
Document Scope
This guide explains the configuration, features and database items that are specific to ClearSCADA’s Mitsubishi driver (see Configuring Mitsubishi Devices in ClearSCADA and see Mitsubishi Data Address Ranges).
It also explains the driver-specific status attributes. These attributes may be useful to system administrators and engineers when investigating unexpected system behavior (relating to the driver) (see Mitsubishi Specific Status Display Attributes).

This guide contains technical information that is intended for users that are sufficiently familiar with ClearSCADA configuration and operation. Before reading this driver guide, ensure that you are familiar with:
- ClearSCADA configuration practices, procedures, and the configuration of properties that are common to many database items. For more information, see the ClearSCADA Guide to Core Configuration, and the ClearSCADA Guide to Core Point Configuration.
- Driver structure, components, and configuration properties, pick actions, and status attributes that are common to many drivers. For more information, see the ClearSCADA Guide to Drivers.
- Simple driver composition, configuration order, and configuration properties and logging options that are common to many simple drivers. For more information, see the ClearSCADA Guide to Simple Drivers.
The Mitsubishi driver enables ClearSCADA to communicate with slave devices and PLCs using the Mitsubishi MELSEC A protocol.
For information on how to configure ClearSCADA to act as a Mitsubishi MELSEC A PLC and report any data changes back to its Master, see the ClearSCADA Guide to the Mitsubishi Slave Driver.
There are no driver-specific pick actions for items on the Mitsubishi driver. However, users with the required privileges can add custom pick actions to a database item by using the User Methods tab on the relevant configuration Form (see Using the User Methods Tab to Define Custom Actions in the ClearSCADA Guide to Core Configuration). See a system administrator for the documentation associated with such custom actions (also known as ‘methods’).
ClearSCADA communicates with Mitsubishi PLCs using Transmission Control Protocol Format 1(see The Transmission Control Protocol Supported by ClearSCADA).
For PLC information not covered by this guide, see the Mitsubishi documentation supplied with Mitsubishi PLCs.
For information on configuring ClearSCADA so that it can communicate as a Mitsubishi Slave, see the ClearSCADA Guide to the Mitsubishi Slave Driver.