Configuring Analog Points

Use OPC XML-DA Analog Points to map analog ‘point’ data on OPC XML-DA servers into ClearSCADA in a format that it can understand, and vice versa.

Configure the properties of each Analog point using the fields on the OPC XML-DA Analog Point Form.

This section covers configuration of the analog-specific properties on the OPC XML-DA tab of the Form.

Use the OPC XML-DA tab to:

For information the Analog Point tab on the Analog Point Form, see Defining Analog Point Details in the ClearSCADA Guide to Core Point Configuration.

For information on the Control tab, see Define the Control Settings for an Analog Output Point in the ClearSCADA Guide to Core Point Configuration.

For more information on the Control Checks tab, see Configuring Control Checks Settings in the ClearSCADA Guide to Core Point Configuration.

For information on the fields on other tabs, see Tabs on Point Forms in the ClearSCADA Guide to Simple Drivers.


Disclaimer

ClearSCADA 2017 R2