Configuring SE Rod Pump Controllers

The SE RPC driver is designed to allow ClearSCADA to interface with Schneider Electric rod pump controllers. The controllers are represented by outstation items in the ClearSCADA database.

The SE RPC driver supports these types of controller (outstation):

If your database structure is ‘modular’ and Group Templates are used to store ‘model’ SE RPC configuration, in addition to the above types of controller, you can add this driver-specific ‘abstract’ controller item to your Group Templates:

You can only add Abstract Items to Group Templates. The abstract items appear as additional driver-specific entries when you display the context sensitive menu from a Group Template. As with other abstract items, in order to represent a ‘real’ controller, you need to convert the abstract items into the required type of controller (outstation) within the Group Instances that reference the Group Template. For more information, see Add an Abstract Item to a Group Template in the ClearSCADA Guide to Core Configuration.

You specify each controller’s properties using the fields on the appropriate SE RPC Outstation Form.

Each SE RPC Outstation Form has several tabs.

Use the SE RPC tab to:

For information on the other tabs, see Configuring a Generic Modbus Controller on the Advanced Modbus Driver in the ClearSCADA Guide to the Advanced Modbus Driver.

For information on the minimal amount of configuration that you can undertake to produce a functional SE rod pump controller in ClearSCADA, see Minimum Configuration.


Disclaimer

ClearSCADA 2017 R2