Using Windows Performance Monitoring Counters

To use the Windows Performance Monitoring Counters you need to :

NOTE: The procedures described are for Windows 7. For other version of Windows and more detailed information about the Windows Performance Monitor refer to the Windows Help.

Further Information

Windows Performance Monitor uses performance counters, event trace data, and configuration information, which can be combined into Data Collector Sets. For more information about the Windows Performance Monitor, see http://go.microsoft.com/fwlink/?LinkId=70270.


Disclaimer

ClearSCADA 2017 R2