Server Status Information
The Server Status Tool provides status information that is organized into groups of categories, each of which contains sub-categories. The Server group provides status information about the server on which you are using the Server Status Tool and it contains the following sub-categories:
- Advise Threads—provides status information about the links from the server to a client
- Advises—provides status information about each server advise connection between the server and clients
- Clients—provides status information about each client that is connected to the server. The number of clients varies according to the size of your ClearSCADA system
- Connected Workstations—provides status information about each workstation that is connected to the server. A workstation is a client and is identified by its Workstation ID.
- Link Threads—provides status information about each connection between the client(s) and the server
- Links (Server)—provides status information about each link from a client to the server.
- Parent Links—
- Parent Threads—