Welcome to the ClearSCADA Installation Guide
Intended Audience
This guide is designed for use by system administrators who are responsible for setting up and managing the ClearSCADA system.
Document Scope
This guide explains how to install ClearSCADA on server and client computers. In this guide you will find information on:
- Required server and client specifications (see ClearSCADA System Requirements)
- Installing ClearSCADA on a server (see Installing ClearSCADA)
- Installing ClearSCADA on a client (see Installing ClearSCADA)
- The different types of ClearSCADA install (see Choose Setup Type)
- The Example Projects database (see Example Projects). This is a database that we have created as a demonstration model. You can install it as part of your system so that you can see examples of how a database can be organized and its items configured.
- Making Changes to your ClearSCADA Installation
- Upgrading ClearSCADA
- Repairing your ClearSCADA Installation
- Uninstalling ClearSCADA.
NOTICE
System will not function correctly
When you install ClearSCADA and Citect SCADA on the same server / client, conflicts will occur between the two applications. The applications will cease to function correctly.
DO NOT install the these applications on the same server / client systems.