ClearSCADA System Requirements

Your ClearSCADA DVD contains the components required to install ClearSCADA on a server and a client. But you should only install ClearSCADA on a server or client computer that meets the required specifications.

In the following sections, we describe the required specifications for server and client computers:

While it may be possible to install and run ClearSCADA on computers that do not meet our recommended specifications, this may result in an unstable ClearSCADA system. ClearSCADA is only designed to run on computers that meet the recommended specifications.

Further Information

Installing ClearSCADA

Upgrading ClearSCADA.


Disclaimer

ClearSCADA 2017 R2