Introduction to the Wonderware Alarm Provider Driver

This driver is a stand-alone driver. It provides additional functionality to enable ClearSCADA to interface with specific supported systems or devices. To interact successfully with such systems or devices, you need to:

Intended Audience

This guide is designed to be used by engineer-level users who are responsible for configuring ClearSCADA to connect to the Wonderware Alarm Provider.

Document Scope

This guide explains how to configure your ClearSCADA system so that Wonderware InTouch can connect to the ClearSCADA Server and retrieve alarms.

The Wonderware Alarm Provider driver enables you to connect Wonderware InTouch to the ClearSCADA Server.

To configure the Wonderware Alarm Provider driver, follow this procedure:

  1. Install the Wonderware Alarm Provider Component.
  2. Enable the connection to the driver in the Server Configuration Tool.

Further Information

Managing ClearSCADA Alarms in Wonderware InTouch.

Configure Wonderware InTouch to Access Database Alarms.

How ClearSCADA Alarm Fields are Mapped to Wonderware InTouch Alarm Fields.


Disclaimer

ClearSCADA 2017 R2